Hello, apologies for the delayed response on this request. To answer these questions:
Yes, you should be able to use 2x MP18851 gate driver ICs for 4x MOSFETs as long as each channel is referenced correctly and is fully isolated (which this solution appears to be).
The MP18551 is ok for hundreds of kHz to the low MHz of high side switching. However, designing around 300MHz of hard switching and assuming FET speed alone doesn’t make sense here. Also sharing driver references across switching nodes isn’t recommended. Fundamentally, you can see how the gate driver switching speed fmax = Idrv / Qg where: