Mid06w0503agy-2s

Hi Team,

Need few details regarding MPN: MID06W0503AGY-2S

• What is the grade of the part, whether it is automotive or commercial or industrial?
• Please share the Material declaration file?
• Can you please share qualification test report?
• Please provide reliability document (which include FIT,MTTF/MTBF)?
• What is the country of origin for this part?
• What is estimated YTEOL for this part?

Hello again Vivek,

The MID06W0503AGY-2S is very similar to the MID06W0505AGY-3R (the -3R is more stringent on the load and line regulation alongside a higher efficiency at full loads), so the details that I am able to share regarding your questions will reflect as such in your last inquiry:

  • This Isolated module is also commercial grade, but it is also UL1577 Certified and CB Certified per IEC 62368-1 3rd Edition.
  • Assuming your question on the grade have to do with operating temps, this IC has a -40°C to +125°C Operating Temperature Range.

For all other questions, you will need to get this data internally. Please fill out the following for more information on this IC: Contact MPS - Contact

Best,
Krishan

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.