Hi,
Ordered a PKT-mEZDPD4506A . Everything is fine controlling it with Virtual Bench. Except that , when I want to set the output > 7V .
MFR_VOUT_CTRL Feedback divider range is set to Range3 (0-6.24V)
Obviously if I try to set VOUT_COMMAND to 7v it gives a warning, and doesn’t allow to write the setup to the chip.
If I change the Feedback divider to Range 4 (0-12.48) then it allows to select any voltage > 6.24V , but the output is exactly half of the desired.
If I select Range5 the output voltage will be quarter of the setted.
How can I configure the device to set the output > 6.24 V ?
Also is there a datasheet with the registers? I couldn’t find it.
The generated DS seems a bit weird to me . Its not clear to me if this device is a single or dual out device. On first page the first sentence contains: its configured for single output. At the package reference seem like it has a second output. VOUT2 . Would it be possible to configure it as an independent dual output SMPS ?