Hi,
In the datasheet of the new MA600 it is shown (see GENERAL CHARACTERISTICS Tab) that the maximum ±3σ resolution (and therefore “effetctive resolution”) that can be achieved is 15 bit.
However, in the online " Magnetic Simulation Tool", I have not been able to reach a resolution near 15 bit (the maximum I could achieve was 12.59 bit).
The setup I’d like is End of Shaft, with a diametrally magnetized ring magnet, using the MA600 with cutoff frequency of 75 Hz.
What setup should I use to get the maximum ±3σ resolution of 15 bit shown in the datasheet? I tried with different sizes of magnet and with simple cylindric magnets but did not have any luck.
P.S.: Please tell me if the ±3σ 15 bit resolution I’m talking about is not the “effective” one.
Best,
Francesco