Hello,
I would like to design multiphase power system which involves these two components.
However MP86957 looks promising, I dont understand why REFIN pin is missing in MPS SPS’s.
This is a voltage input pin controls Vcm of Iout pin.
there is a formula to calculate Vcm voltage. According to that formula
0.7<((Isw*Giout)*Riout)+Vcm<2.1
- Vcm value is between 1.52-1.68 on LTC datasheet.
- Giout is 5uA/A
- Isw ~30A
To calculate Riout
0.7< ((30A*5uA/A)*Riout)+1.6<2.1
Riout<~3.3k
So if I use a resistor below calculated value Can i achieve that missing pin problem ?
or is there a another solution can help me about REFIN pin problem ?
BR,
Mustafa.