Is Constant Current(CC) and Constant Voltage(CV) is controlled by the IC HR1211

Is the CC and CV mode is controlled by the IC HR1211 or the TL431 shunt regulator.

Hello,

Generally speaking, the controller should be what controls the operation mode; either CC or CV. The HR1211 is an AC-DC controller that combines PFC and LLC in one package and it should be the one controlling the operation mode.

If you are using these parts in a charger design, this reference design article may be helpful if you have further questions.

Offline 600W Battery Charger / PFC + LLC with HR1211

We also have an evaluation board for this circuit which is EVHR1211-Y-00B.

Feel free to reach out if you have further questions.

Thank you,
Eliza