Questio is if I change the R116, which is used to set the Ilim current, the SW frequency only chang a little,
I chage the R116 from 49.9k to 82k, SW frquency change from about 13kHz to 23kHz,
does there any detail doc how can I change the SW frequency to 100kHz or higher, thanks
Yes, the Fsw is affected by the peak current limit set by the resistor on Ilim pin. Please look for the section where it says " Maximum Switching Frequency" in the datasheet, and use the equation 14 to calculate the Ilim with respect to the Fsw you need. Then using equation 8, you can determine the R3 for the application.