Hi
Is there a way to calculate the Loop Bandwidth.
This is my schematic
It would be great, if there is a formula.
Thanks
Kind regards
Frank
Hi
Is there a way to calculate the Loop Bandwidth.
This is my schematic
It would be great, if there is a formula.
Thanks
Kind regards
Frank
Hi Frank, the datasheet has typical values for the FB and RT resistors for a 5V out application that put the bandwidth in the correct place. Can you try these values?

Hie Kareem,
thanks but with the proposal from the datasheet, the required phase margin (for a stable system) is smaller than 45 degree.
Here is my solution (best compromise).
Instead of 22.1kOhm I take a 22kOhm resitor.
So I have values from E48 row.
Hi Frank, the reason the phase margin is reduced in your original setup is because of the pole introduced in the feedback loop with C6.
If you simulate the recommended values from the datasheet for Vo = 5V, you should see a healthy phase margin of roughly 53 degrees.
Hi Frank,
It is possible but we would still recommend keeping the phase margin above 45 degrees for better stability.