Hi
We are considering using MP5031 as USB-C PD controller together with communication on the D+ D- line, but we are worried that the precense of MP5031 connected on D+ D- corrupt data communication.
Normally it is not good practice to have several paths of D+ D-, for signal integrity.
Is is possible to use MP5031 without connection to D+ D-, only supporting “normal” USB-C PD?
The DP/DM pins are used to determine the charging mode. Depending on what charge mode you want you would be requiring the DP/DM connections.
You can follow the layout guidelines from the DS for optimal performance.
If you’re using USB A then DP/DM will be used. If you’re using type C, CC line will be needed.
I believe you would need the CC lines since you want type C on the hub. CC lines are for discovery, configuration and management of connections across a Type C cable. USB A pin out has D+ and D- which cannot be connected to CC lines. These get connected to DP and DM respectively.