EVL8870-L-00A (EVKT-USBI2C-02) DRIVER and GUI for evk board evaluation

Hello,

I got the MP8870 DEMO board with the MPS EVKT-USBI2C-02 adapter . Unfortunately I can’t find and install the right usb-i2c driver for this board and also can’t find the GUI software which I need in order to evaluate device performance (efficiency, ripple, load transient, etc).

Will appreciate for help/ guidelines,

Thanks,

Igor

Hi Igor,

If you already have the Communication Interface Device (EVKT-USBI2C-02), the only thing you have to do now is download the GUI software available on the MPS website (Virtual Bench Pro 4.0). Once you download the software and connect the board using the communication kit, you should be able to Scan or Manually Add the part number and access it.

Let me know if you have any other questions!

Best,

Gabriela

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.