Hi,
I have the EVCS1805-S-00A Current Sensor Evaluation board and I am using it to measure current in my circuit. My current measurements are 2V off. I’m using an electronic load to verify my current measurements.
- In the datasheet of the EVCS1805-S-00A under the performance summary, what does VOUT for bidirectional options mean vs VOUT for unidirectional options?
- Right now I am test DC current but I will need to test AC current. How can I do so? Is that what the bidirectional vs unidirectional options are referring to? I’m guessing that I don’t have to make any changes on the board it’s just a matter of the calculation, right?
- In the datasheet, VOUT for the bidirectional option is:
VOUT = .1 VCC + Sens Ip
This means Ip, the current I am sensing, is:
Ip = (VOUT - (.1 * VCC))/ Sens
If VOUT is 0V because there is no current then Ip doesn’t equal zero based on the equation.
(0 - ( .1*3.3))/.00264 V/A)
What am I missing? Is the calculation wrong? Please tell me the correct equation for calculating the current for both DC current and AC current.