Hello! I am using the EV6540H-U-00A – 6A, 50V THREE-PHASE BLDC MOTOR DRIVER EVALUSTION BORAD in one of project to drive BLDC HUB motor) but I noticed that the nFault goes low much too often. I run the motor at low speed for a few seconds, the temperature is very low, the PWM duty cycle is always below 10%, the current monitored at the SOx pins never goes above 1.5A and yet the nFault is triggered very often. What are other possible error conditions? I am using 24V SMPS to drive motor.
Expecting quick response
Thanking in advance