I have purchased the EV3305DD-00A based on the MP3305. I am using the evaluation board which says it is optimized to drive 3 white leds in series, 10 in parallel. The value of C5 is 2.2uf, 25V.
However, I am using this eval board to drive 8 white leds in series only with a maximum total forward voltage of 25.6V. Based on application circuits shown in the MP3305 data sheet it looks like I should change the value of C5 to 330nF, 50V. Can you confirm? Or provide another value? And changing R5 to 330K for OVP?
Please let me know of any other recommended changes as well.