Hello, I will use MP2617H to our IoT devices production. I ordered EV2617H-L-00A evaluation board. First I tested with 12V input. I used 1000uF capacitor at VBATT pin as a battery. VSYS and VBATT output is OK as specs.
But after few tries, VIN not powered to VSYS and VBATT. I use 12V input, Li-ion 1S battery, jumpers M0 and M1 are HIGH, EN jumper is LOW. ISET, NTC,pins are float on the board. I got 4.47V from VCC when VIN is 12V. But it didn’t charge battery and supply VSYS. Board is only supplied power to VSYS when battery is connected. If I detached the battery it didn’t use to VIN for supply VSYS. What is wrong ? Can you help me about this issue.