Could you provide/add a dimension drawing for the evaluation board. I do not see this information in the datasheet EVL8030-QJ-00B Rev. 0.8 I’ve downloaded the Altium PCB file but as I don’t have Altium it is not easy to get the dimensions of the PCB or the location of the mounting holes.
Hello Ron,
Welcome to the MPS Forms!
The datasheet does mention that the dimensions of the whole board is LxWxH (16.2cmx5cmx2cm) with the actual package size being QFN-32 (5mmx6mm) package.
These dimensions if manually overlayed on the board using CAD (whatever you are able to access if not Altium) to get the best estimates for pinpointing the dimensioned locations for the mounting holes.
There is a PCBDOC file on the main page of the EVL8030-QJ-00B under Design resources that can also help with this. Opening the file in Altium Designer or any other PCBDOC compatible softwires should work.
Hope this helps.