Hi Support
I am looking for detail design guide for VOSNS+ and VOSNS- of MPM3695GMQ-10-xxxx. For example,
(1) I want to understand how long we can route the VOSNS+ and VOSNS- between load sensing point and regulator?
(2) what’s the parasitic requirement for VOSNS+ and VOSNS-? Do I need to route like 50 ohm transmission line? or is the only requirement is resistance and what is the target value?
Hi Tim,
One of the team member will reach out to you soon via email to help support you.
Thank you
Saurabh
Hi
Could you please upload the EVM design schematic on the website?
Hi
Can I get some update for the support?
Hi @tim.peng,
So sorry for the delay here.
Please find the response for your questions below:
-
It is hard to provide a specific guidance on the maximum distance between load and regulator. It depends on the impedance of the distance. If the impedance is too large, oscillation may occur. We usually add a 10nF capacitor across VOSNS+ and local output to eliminate this oscillation.
-
No resistance is required for VOSNS+ and VOSNS-. You may route them as differential lines and keep their resistance similar.
One our team member will contact you soon via email with the EVM schematics. I have forwarded the contact information.
Thank you for your patience.
Saurabh