DCDC Converter Selection Help

Hi,

I am looking for a DCDC buck/boost converter that can take in 3.6V and output 36V. It needs to be able to provide 5A at a peak current option to my device as well. I am planning on using batteries that provide 3.6V and up to 30A to then convert to 36V with a peak of 5A. It is to power a PCB board that has motor control to power a separate motor. Please let me know if you have any DCDC converters that might work for this and how I could configure them for my project.

Thank you,

Monique

Hello Monique,

Welcome to MPS Forums. Based on the given specifications, MP4248 might be a potential fit for your application.

1 Like

Thank you! It does look like I would need to set the OTP settings to be what I desire as well. When I receive new chips from MPS, how do I set my own OTP settings rather than using the default ones?
Thanks,
Monique

Hello @mdubois3 ,

The default part has fixed register setting stored in the OTP(one-time programmable) memory. For a customed OTP settings, a new suffix code pertaining to your desired register settings needs to be generated. Please submit a ticket via the form below.

Thank you,
Before I do that, I want to test it via reprogramming in real time via the web bench. Can I input 3.6V and then change the output to 36V, and then adjust the switching current limit?

Is there someone I can discuss my proposed design with?

Hello,

I reached to your email earlier today.