Hello
Can not add new component in databases.
- DC/DC Designer 3.21 (installed on default location)
- Window 11
- c:\Program Files (x86)\MPS\DCDCDesigner 3.21
read-only disabled
– Best Regards
Victor
Hello
Can not add new component in databases.
– Best Regards
Victor
Hello Victor,
It would be best to find an inductor of similar inductance to the one you wanted to use. Just make sure saturation current is rated properly and if the DCR is different just remember it will slightly affect the efficiency plots generated.
Regards,
Jonathan Hidalgo
You’re absolutely right. When replacing an inductor, it’s crucial to match the inductance as closely as possible to ensure the circuit functions as intended. The saturation current should indeed be rated properly to avoid inductor saturation at high currents, which could lead to malfunction or damage. Autodesk Civil 3D 2023 software buy. Additionally, a different DCR (Direct Current Resistance) will affect the efficiency, as it impacts the I²R losses in the circuit. It’s always good practice to consider these changes and how they might alter the performance of your design.