Hello!
I have a problem, where my electronics needs 5V regulated power supply from an input, which varies between 5V and 20V. This input source is a regulated 5V most of the times, but occasionally it is increased to a higher regulated voltage like 9V/15V/20V for several hours.
Your MP8715 IC seems to be a perfect solution to me, as if I understand the datasheet correctly, it can act as a “pass-through” device with the 100% duty cycle feature when the input is the regulated 5V, and in case of the higher input voltages, it’ll regulate the output to 5V.
However just to be sure, I would like to ask for some clarification.
Regarding the bootstrap capacitor and its charging circuitry the datasheet has two statements:
In the electrical characteristics (for 12V input voltage) it says that the BST Under Voltage Lockout Threshold (BSTUV_Vth) is typically 2.8V.
In section “Floting Driver and Bootstrap Charging” it says that: “The floating power MOSFET driver is powered by an external bootstrap capacitor. This floating driver has its own UVLO protection. This UVLO’s rising threshold is 2.5V with a hysteresis of 150mV.”
I did not find anywhere that for what should we reference this UVLO. I assume that the VIN should be higher than the mentioned values, however I want to be sure that not the (VIN-SW) voltage should be higher than the mentioned values.
Therefore I would like to ask that am I right, that the voltage of the VIN pin should be higher than this 2.5V/2.8V in order to the bootstrap capacitor charging to work properly?
Additionally, I would like to ask, that is there any minimum output current requirement for the MP8715 to operate properly in 100% duty cycle mode?
Thank you,
Ferenc