Charge Enable Conditions for MP2602

I am working with a customer who has integrated the MP2602 single cell battery charger. The design has the following parameters.

VIN = 4.3V
RCHRG = 2.3k

I’m observing that in the design that after the battery is fully charged (e.g. 4.10-4.15V), the MP2602 appears to not begin a new charging cycle until the battery voltage has decreased to ~3.85V. That is much lower than we expected.

With the VIN of 4.3V, the 2602 detects a valid input power as the PG pin is pulled low. The charger is enabled via a resistor configuration.

Would it be possible to provide more detail about how the MP2602 makes a determination of when to begin charging a battery? Is there a hysteresis value in the charger than needs to be below a certain voltage threshold?

With the fairly low VIN value, it is understood that the charge current will be limited or reduced and that is acceptable in this application.

Thank you!

Hi Carl, Welcome to MPS now forums!
My team and I are working on this, we’ll get back to you as soon as possible. Apologies for the delay and thank you for your patience.

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.