Charge Controller suggestion to Charge lifepo4 Battery 80A

Hi,

We are looking for recommendations on a suitable topology and charge controller for charging a LiFePO₄ battery with the following requirements:

  • Input voltage: 9–36 VDC

  • Output voltage: 10–36 VDC

  • Output current: up to 80 A

We understand that a single IC may not support this current level, so we are considering a parallel architecture using multiple controllers. Kindly suggest an appropriate approach and suitable IC options.

Thanks,
BK

Hi,

Welcome to MPS forum. We don’t have a solution for 80A charging current. If you have any other questions please let me know. Thanks for reaching out!

Best,

Fox

Hi Fox

Please suggest Charger IC to support below Baatery

16 Cell

Lifepho4.

Charming current max=4A

Automatic full MPPT Support.

Input : PV Solar. 24V