Boost Topology of MPQ24833

Hii MPS team,
I need Calculation sheet of MPQ24833 in Boost application.
Please, if possible, send it to my mail nitin.tejaswi@forvia.com .

Also kindly specify me that "what is the max output voltage of this IC, if I will do boost at 9-32v input voltage.

BR
Nitin Tejaswi

Hi Nitin,

The max output voltage is decided by the maximum duty cycle and minimum on time on the datasheet. The frequency is fixed 420kHz for MP24833-B and 210kHz for MP24833-A, you can calculate the max Vout.

What kind of Calculation sheet do you need? If you want to know how to select the components, you can use our EVB datasheet as a reference. And there are also some instructions on the MP24833-A datasheet page 10 and 11.

If you have any other questions, feel free to ask me!

Best,
Fox