Hello.
I measured the Bode plots and load step response.
The phase margin was about 20deg and the ringing frequency of the load step response waveform was more than 7 times, although it might be due to the load capacitors connected about 2000uF in total.
Normally, when measuring Bode plots, the injection amplitude is set at 10 mVpp. When the injection amplitude was set to 100 mVpp as a trial, the phase margin satisfied 45 deg. The amplitude of the load step response waveform was also about 10 mV. Due to the limit of the current that can be injected, it was not possible to input a larger amplitude than this.
Please let me know how much is the correct injection amplitude for Bode plots measurement and load step response waveform measurement of MPM3690-20B with COT control.
I have a further question.
There is an argument that COT control is, in principle, guaranteed to be stable. If this is the case, does it make sense to use bode plots to determine the phase margin?
Hello.
It has already been two weeks since I first asked the question and I have yet to receive a reply. I would appreciate it if you could give me some perspective. Best regards.
Hello Hayami,
This is most likely a product of bad layout. On our DS, we use 1380uF total and got a much better transient response. Try to keep output voltage traces with minimum impedance, by making traces wider and/or shorter. A large amount of inductance could be coupling with the parasitic capacitance which results in ringing.
With regards to COT - A bode plot is not the best way to measure its stability / performance, since bode plots only work for LTI systems. Best way would be to look at transients.
Regards,
Jonathan