I’m looking for a charger IC for the battery backup solution with power path:
- Charging 1 cell type Lithium polymer
- The maximum power available at the input is a regulated 5V 3A
- The system loadis up to 2.5A
- At full power the charger must disconnect the main power to prioritize the battery
Hi vzlosnikas,
We have several 1 cell switching chargers available.
What is your end user application? Are you looking for OTG mode?
I would like to recommend MP2722 which should cover your requirements, kindly take a look at this article as well for more understanding.
We do have several other 1 cell switching chargers, that you can take a look at. Since you have a load/charge current upto 2.5A, I will not recommend using linear chargers.
Let me know if you have any more questions.
Regards,
Adhish
Hello Adhish,
Thanks for your fast response.
Maybe I caused some misunderstanding when I mentioned 5V. We do not need USB. Our system operates at 24V, and we will step it down to 5V to power both the charger and the system.
Regards,
Valerijus.
Hi vzlosnikas,
I guess in this case, I can recommend you using our standalone buck charger part MP2617H which has a power path management.
Also, FYI this part also has A & B version which has a max operating Vin of 10V and a slightly lower discharge current than H.
Let me know if you have more questions.
Regards,
Adhish
1 Like
This topic was automatically closed after 6 days. New replies are no longer allowed.