Dear support member.
Please teach me what is analog mode.
If I set external divider without PMBus and setting ROM.
In this case. Is this MPM3695-25 output Voltage decided with equation(1) ?
or Am I need to write settings on ROM?

best regards.
Dear support member.
Please teach me what is analog mode.
If I set external divider without PMBus and setting ROM.
In this case. Is this MPM3695-25 output Voltage decided with equation(1) ?
or Am I need to write settings on ROM?

best regards.
Hi Ryota,
The external divider takes priority over PMBus operation for the output voltage. Equation 1 will help you choose the resistor values to set for Vout. No need to write anything to the ROM.
Hi Cecilia
Thank you for answer.
Hi Cecilia
I have add question.
I want to use current sense with virtual bench pro 4.0.
In this case can I using analog mode?
best regards.
Hi Ryota,
It should still be able to read the output current in analog mode in the GUI.
Hi Cecilia
Thank you for answer.
I have add question.
Please teach me how to set this device set to analog mode.
I tested analog mode on EVK.
but It’s not work analog mode.
I’m setting to OTP with GUI and setting the external divider.
In after I turned off power and turn on the power with out PMBus.
In this case it looks to the OTP’s priority is higher than external divider setting.
when I use otp once time can I seting to analogmode?
best regards.
Hi Ryota,
Since the MPM3695GRF-25-0022 has the default settings for internal divider, you will have to set it to external divider and write to the non-volatile memory (NVM).


Hi Cecilia.
Thanks for answer.
I have some question.
1.How default setting values of MPM2316-25-0022.
I understand to need to setting the External divider (D1h) setting.
the Datasheet is written the default value that is already setting External divider.

In this case, Can I use analog mode without setting NVM.
or I need to set NVM?
2.When Virtual Bench Pro4.0 with analog mode.
I can see output Voltage is 0.72V with Oscilloscope when I set register to default value and selected register divider for Vout = 0.72V.
but Virtual Bench shown output voltage is 1.8 V
best regards.
Hi Ryota,
Hi Cecilia.
Thank you for answer.