Hi,
Can the MP2148 support two output voltages by using a discrete FET to switch in a resistor in parallel to one of the feedback resistors? The idea would be to have the part default to Vout=0.8V, and then when the FET turns on it would change one of the feedback resistors such that Vout=0.9V. Any concerns with this approach? Is there a better approach I should consider?
-Matt