Dear support team,
We are developing a system using MP2650, 2S battery and USB PD charging, system diagram as show below.
In the system we have a low power MCU powered from MP2650 VCC pin. When system is powered by battery only and in off mode, we set MP2650 REG0Bh[1:0] to 00, disable PROCHOT and PSYS, also put MCU in sleep state.
If user click ON button, the MCU wakes up and subsequently turns on the main processor.
Our questions are:
- When MP2650 is in battery only and lowest power mode, can the MCU access I2C registers to turn on ADC and read battery voltage?
- When MP2650 is in battery only lowest power mode and MCU is sleep, when AC adapter is connected, will ACOK assert and can we use this to wake up the MCU?
TIA
Bob