Hello,
I saw to another person Question which topic is double Iout. (MP4575 - Two ICs in parallel mode to double the Iout)
(link : MP4575 - Two ICs in parallel mode to double the Iout)
As a power system used in a vehicle, we will use two MP2908A to build a DC-DC converter that supports high current.
If you have a typical schematic or applicaion note, please share it.
- request
- Please share the schematic and application note of 2 MP2908A that supports high current.
- Please tell us if there are any precautions or notes when connecting 2 MP2908A.
- I would like your e-mail address for direct contact.
The specs you want to use are as follows
Vin : 12~48V
Vout : 8V
Iout : 30A(Peak) / 20A(Avg)