I am using the MP6531A. According to the datasheet, it states that nFAULT is driven low when certain fault conditions occur. My questions are as follows:
- I would like to confirm whether nFAULT is asserted low in each of the following cases:
-
When VIN UVLO occurs
-
When VREG UVLO occurs during the initial start-up
-
When VREG UVLO occurs while the motor is running
Please advise.
- If nFAULT is not asserted low for the three fault conditions above, the MCU may continue outputting PWM without realizing a fault has occurred. In that case, is there any way for the MCU to detect these faults? Any suggestions would be appreciated.