Power rating of resistor in MPQ4228-Q datasheet

Hello! Thanks for your reply. For the reference, I do not want it to go above 12V 1.5A (~20W) because the input of the MPQ4228-Q will be a stable 12.92V source capable of only up to 2A (~25W), until thermal throttling, so I will stick to the default 5V3A, 9V2A and 12V1.5A. Thanks!