MPQ5069 behavior under "high" load

Yes, it’s heatsunk. Based on the power loss vs load current graph, and the efficiency one, does that mean that Rds is irrelevant? Its spec is 7-12mOhm however if we’re at 8A and worst case Rds, that would give 768mW, not the 1.1W or more shown in the graph, and better than 99% efficiency. Where is the disrepancy coming from?