Hi,
I created a board with several MPM82504 in different configurations on it. Our plan is to configure them onboard via PMBUS using our own tool chain. Now I am preparing the register configuration using the Virtual Workbench V4. Because I do not have the boards available, I can not scan them (with MPS USB I2C adaptor) and need to add every device of the powertree manually. But when I add them only Channel 0 is shown but not the other 3 Channels. I could not find a way to add the other channels. It is the same for the Virtual Workbench V3. How can I add these other channels?
Thanks in Advance.
BR,
Denis