Hello,
I was wondering if I can receive a little more details about the capability of MPM6010. So, in its datasheet it is specified in the typical performance characteristics chapter that it works with 2 series LEDs which have a forward voltage of 6V together and also, all the typical application schematics have 2 series LEDS connected at the output. So my question is what is the maximum number of LEDS that could be connected to MPM6010 or can I connect how many LEDs I want as long as the output current doesn’t exceed 1.5A? Does this apply even to chip LEDs which have for example 2 LEDs on one chip?
Thank you very much!