There are 9 MPM54304s on my board, and some of the devices will fail to respond to the first IIC communication when powered on, but the following communication will succeed. The positions of the components which fail are random and vary with each power-on.
It seems that the power-on initialization process is improper, causing the IIC state machine to be abnormal.
Can you provide some Debug methods?
Hello hongyuc,
Is it possible for you to check if the startup input and pull up voltages proper?
Is there any droop that causes the devices to go in UVLO during startup?
Can you check what the first initial i2c communication data is?
Does our Virtual Bench Pro 4.0 show any faults?
Regards,
Vinh Tran
Hi vinh.tran,
Please check the results as follows.
Since I can only attach one picture to each reply, I have to reply separately.
Is it possible for you to check if the startup input and pull up voltages proper?
Is there any droop that causes the devices to go in UVLO during startup?
The input voltage stays stable before the first IIC commucation.
Can you check what the first initial i2c communication data is?
Power up overview:
Does our Virtual Bench Pro 4.0 show any faults?
Sorry,we don’t have the USB Cable
Hello hongyuc,
I2c startup looks fine to me.
You can see the PMBus message format on page 27 figure 7. The initial connection looks to be Start, Address, Write, NACK, then Stop. This looks to be just the acknowledge process upon i2c startup. It looks to be not acknowledge. Please check if you have the correct device address in the firmware.
Regards,
Vinh Tran
Hello Hongyuc,
You are correct, I was looking at wrong information. MPM54304 does not have PMBus. Only i2c.
Can you confirm that the VCC is above 2V for all device when the i2c communication starts? It is possible that the the internal circuitry is not working properly because Vcc is not >2V yet.
Does this i2c communication failure occur during operation too? Or just at startup? Is this the only device on the i2c lines?
Regards,
Vinh Tran
Hi vinh.tran
I added Vcc to the test:
Yellow: Vin (12V)
Red: Vcc (3.3V)
Blue: SCL
Green: SDA
The failure only occurs at startup, and MPM54304 is the only slaver on the I2C bus.