Hello everyone!
I would like to use MP9486A in an automotive BMS application and I was wondering what the minimum output voltage would be? I would like to use it with a 3.3V output.
The specs for my application:
VIN range: 45 - 75.6 V
VIN nominal: 66.6 V
Iout(max): 1A
Iout(nominal): 250 mA
Vout: 3.3V
Do you think this would be possible with MP9486A?
Thank you in advance!
Greetings,
Peter