Mp8008, mp8009 Transformer

Looks like it, the only ratio in the transformer that has changed is the secondary winding. Looks which is double the 12V version. So the reflected flyback voltage will be the same as the 12V version and the tertiary voltage will be the same as the 12V version. Voltage ratings of output caps do need to be observed