EVQ7228-QJ-00A Load Forward Voltage Adjustment

I’m trying to use the output not with LEDs, but with another type of load. The voltage drop across my load is about 1.8 V, but it doesn’t turn on the channels. However, if I connect, for example, two LEDs in parallel, it works. Is there any way to configure or program the chip so I can power a device that has a 1.8 V voltage drop?